我在做boost升压电路时,用TL494输出的单个pwm波C1端口输出来控制三极管tip122的关断,占空比48%,三极管这部分是单独搭出来的boost拓扑,没有反馈,给了输入后,设定数字电源输入12V,3A,输入上显示的是5V,3A,三极管发热厉害,这是什么原因,我对boost拓扑还有一个疑问,在boost拓扑中,开关闭合后,电路中只有电源,电感,开关(闭合),这样不就相当于短路了吗,这一过程电流岂不非常大
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Boost的下管开通只是On time时间里,电感电流会上升,但到Off time,电感电流又会下降,所以这个过程跟短路是完全不同的。你之前应该没有做过电源,建议找本电力电子教课书,研究下拓扑的原理。你的电路从你的描述看,输入电源过载了,1)检查下TL494的C1输出是否为48%的占空比;2)二极管一般不适合高频应用,所以你的驱动频率多少;3)其他问题
您好,請問切換頻率設定多少?開關導通時,電感電壓等於輸入電壓,電流線性上升,只要電感不飽合,就不會等於短路,低頻時電感是等於短路,高頻時不等於短路