Other Parts Discussed in Thread: TPS62130, TPS62136, TPS563200, TPS563209
TPS62130能够支持宽电压3V~17V输入,3A输出。但TPS62130的RDSON分别为90mohm, 40mohm, 还是比较大,效率不够高,有没有效率比TPS62130更高的且宽电压,3A的器件?TI的产品线是否有在开发?谢谢。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
你好,你是一直重载工作么?你对效率的要求是多少?v这个芯片效率在重载都是超过90%, 轻载条件下,效率的确很低,如果你需要轻载高效,建议选用带Eco-mode的芯片,可以实现轻载时50%左右的效率。
重载条件下,注意电感的选取,DCR过大也会降低效率