在webench designer中为什么找不到TPS61194的模型?f=495.6KHZ,输出电压28V,电流4*80ma,输入电压7~16V,在这些条件下计算处的电感L1值是85UH,是否有问题,最好告诉我在哪里可以仿真TPS61194
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
在webench designer中为什么找不到TPS61194的模型?f=495.6KHZ,输出电压28V,电流4*80ma,输入电压7~16V,在这些条件下计算处的电感L1值是85UH,是否有问题,最好告诉我在哪里可以仿真TPS61194
Hi
Webench 暂时没有包含TPS61194这样的多路LED驱动设计,所以无法用这个软件仿真。
这个器件主要的设计就是电感,可以按照一般boost 架构那样计算,其他相关计算建议参照EVM板: http://www.ti.com.cn/cn/lit/ug/snvu492/snvu492.pdf
电感可以用68uH. 饱和电流建议大于2A.
目前没有软件支持它的仿真,关于电感取值,参考数据手册就可以了。最好可以用EVM进行实际测试