请教一下,TI 降压芯片,是否有 输入5-30V ,输出是正负12V,正负15V。2A左右的芯片。
我现在需要实现的是输入24V,输出正负15V,2A,用于音响电源上。
想要个DC TO DC的负电源,替代LDO稳压IC 79系列的,TI有吗?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
你需要明确你的输入电压,而不是5~30V,以这个电压,你之前是无法用LDO实现,选型起来相对麻烦。
如果确实需要5~30V输入,用2个芯片做,例如升降压芯片LM25118, 负压可以用降压芯片做成升降压负输出,例如TPS54560(甚至要更大电流的降压芯片,这个还是要取决于你的输入电压)