UCC3895的推荐频率为200KHZ;希望推荐一款IGBT:Vce:1000V~1500V;Ic:40A~120A(80A~120A);及相关的IGBT驱动IC或者方案?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
你好,
我们公司有IGBT driver,ISO5500
Drives IGBTs up to IC = 150 A, VCE = 1200 V
是隔离型的驱动器,完全满足您的应用需求。
目前还没有IGBT产品