This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

lm2674输出电压不稳

Other Parts Discussed in Thread: LM2674

最近使用lm2674将24V转换为6.8V,采用手册中推荐电路。其中Cin、Cout均为47uF,L为47UH、Cb为10nf、D1为SS16。R1、R2分别为10k、47k,使用100nF电容与R1并联。上电后输出电压为2V,反馈电压0.3v,过一会儿输出电压恢复正常。

再次焊接一块板调试,去掉与R1并联的100nf电容,输出依然为2v,将此电容值连续更换,会出现输出为20v的现象,有时输出会先过冲到20v,然后降为2v,总之不论怎么改,输出电压不能达到6.8v。后来换为68nf,输出正常,再将电容换为100nf,输出也正常。后来将电容换为10nf-1uf之间的值,上述输出不正常的现象不能再复现。

这是因为什么呢?