Hi,
最近在调试一块BQ24253的板子,这部分原理图如下:
实际板子上有几点改动:
1、D+/D-短接了;
2、D1 LED灯改成了10K电阻;
3、R16改成了165R电阻;
4、电池是一颗103040型号的1200mAh 3.7V锂电池,没有TS管脚,所以PIN9没有接;
外部MCU在上电时会把CEn,EN1,EN2都初始化为LOW,检测到PGn为LOW后,MCU会把EN1拉高,现在的问题是CHGn这个管脚输出始终是高,没有进入充电模式,实测也没有充电电流,请问是什么原因?谢谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
最近在调试一块BQ24253的板子,这部分原理图如下:
实际板子上有几点改动:
1、D+/D-短接了;
2、D1 LED灯改成了10K电阻;
3、R16改成了165R电阻;
4、电池是一颗103040型号的1200mAh 3.7V锂电池,没有TS管脚,所以PIN9没有接;
外部MCU在上电时会把CEn,EN1,EN2都初始化为LOW,检测到PGn为LOW后,MCU会把EN1拉高,现在的问题是CHGn这个管脚输出始终是高,没有进入充电模式,实测也没有充电电流,请问是什么原因?谢谢!
Hi
TS电压必须在规格(30%~60% VLDO之间)反馈内才能正常充电。
Hi,Johnsin:
TS电压调到约50%后,可以正常充电了,谢谢!