请教大家一个问题,我用的bq78350R1+bq76920,采用NCR18650BM 3200mAh 四串两并的电池,这里电池的放完电的电压应是2750mV,我这里出现的问题是电池充满后做放电,放到电量51%的时候,两端的电压到3500mV,然后接着就直接跳变到7%了,电量就只剩300多mAh了,我想知道应该怎么设置使电量校核准确,怎么去设置Pending EDV的值
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
请教大家一个问题,我用的bq78350R1+bq76920,采用NCR18650BM 3200mAh 四串两并的电池,这里电池的放完电的电压应是2750mV,我这里出现的问题是电池充满后做放电,放到电量51%的时候,两端的电压到3500mV,然后接着就直接跳变到7%了,电量就只剩300多mAh了,我想知道应该怎么设置使电量校核准确,怎么去设置Pending EDV的值
还要检查一下你用的是fix EDV还是CEDV。
如果是fix EDV,要看看是不是电芯不均衡,有其他的电芯电压低于2900mV 了