Other Parts Discussed in Thread: TPS54A20, LM25141
需要一款DC/DC电源转换芯片:输入电压为12V,输出电压为5V(或3.3V),输出电流10A,转换频率为3MHz的电源转换芯片,请推荐。谢谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
tps54a20: http://www.ti.com.cn/cn/lit/ds/symlink/tps54a20.pdf
不过这是个2相降压芯片,最大输出电流10A,单相频率是2~5MHz, 但是这个芯片最大只有2V的输出,不合适。
其他芯片频率要么最高到2.6MHz之类, 例如LM25141之类,不过这类外置MOS的芯片,频率高容易造成功耗高。
请问为什么要3MHz这么高频率?
(在降压芯片List中设置最大频率大于2000kHz,即可得到: http://www.ti.com.cn/zh-cn/power-management/non-isolated-dc-dc-switching-regulator/step-down-buck/products.html#p451max=8;420&p20max=2000;10000, 但是看起来并没有合适的)
为什么要3MHz频率?你是用在汽车上么?
输出电流这么大,频率很高的话,芯片会发热严重,所以一般的高频芯片都没有这么高的带载能力。
除非你是多相位并起来实现10A。
54A20输出电压最多可以到2.8V(单项2MHz)