This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS25740B 问题咨询

Other Parts Discussed in Thread: TPS25740B, BQ25895, TPS25740, LM5175

Dear 

有个客户在做Type C PD 的选型,要求支持4个电压点。我们建议了TPS25740B,但客户提出了如下几个问题,我们是否都可以满足 ?

a: PDO 是否可以客户自己配置,比如这颗IC 可以提供3A,但客户自己可以改成对外广播成2A最大电流
b:
是否有端口指示IC 是工作在输出5V 或者是输出PD 状态
c: IC
是否可已设置成输出电压只有5V 9V的输出
d: PD
方案是否有针对Apple Mac book, Mac book pro,Ipad 的测试数据,主要是担心兼容性上有问题
e:
是否有方案可以给电池充电,且可以给电池放电,并且支持PD的规格,我们BQ25895 这些方案,不支持PD,是否有类似于BQ25895+PD这种合在一起的方案