In the DS of LM74700-Q1, Section Absolute Maximum Ratings, Do not have the min vlaue of the CATHODE pin.
Now, In my application, it may be have a negative voltage(-36V) on the CATHODE pin, is it ok?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
In the DS of LM74700-Q1, Section Absolute Maximum Ratings, Do not have the min vlaue of the CATHODE pin.
Now, In my application, it may be have a negative voltage(-36V) on the CATHODE pin, is it ok?
Hi
没有问题。
CATHODE脚的电压实际受制于ANOOE的电压,因为两者之间之隔着一个导通的MOS管。
你好,感谢回复
关于你的回复,有点疑问,
放从A端输入一个-36V时,此时MOS管也是不导通的,由于MOS体二极管的存在,C端应该是0V
当从CATHODE输入一个-36V时,A端没有输入,MOS管是不导通的,这时由于MOS体二极管的存在,应该是A端电压跟随C端,也为-36V
Hi
你的意思是输出C端有-36V, 而此时输入端没有输入或者说是0V, 你想判断这样情况下芯片是否有问题吗?
对的,我们的应用场景就可能会出现 : A端没有输入,而C端可能会出现反接,即C端接上了-36V
我想知道这时候,芯片会不会损坏