This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ24070,不良品太多,充电电流有的可以达到要求,有的不可以

如图为设计的应用电路图,V(DPPM),设定在4.3V,充电电流设定在1.5A,批量生产后,发现有一半的设备在给电压为3.8V左右的电池充电电流达不到1.5A,有的为0,有的只有0.2A,有的为0.5A,有的正常,能达到1.4A,以上的测试情况均在输入电压足够的情况,也就是DPPM并不应该启动的情况。另外还发现有的芯片在输入电压在4.5V的时候还是正常的,充电电流可以达到1.5A,但当输入电压再调高一点,充电电流瞬间降到只有0.2A左右,并不时的再0.2A和1.4A之间跳动。把电压降下来,又恢复正常。另外还发现,把充电电流不符合要求的RDPPM换成33K的电阻充电电流恢复了正常,但却牺牲了输出电压VBAT。

电路板外围器件没有问题,因为我们把好用的芯片拆下换掉不好用的,充电电流就可以正常。

难道真的是芯片质量有问题,还是设计的有问题?