This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

单独使用EMB1428驱动开关管的程序调试问题

Other Parts Discussed in Thread: SN74LVC2G14-Q1

本人单独使用EMB1428驱动开关管,程序调试的时候发现以下几个问题:

(1)请问上电顺序很重要吗?能不能让VDDCP、VSTACK以及12V、5V、3.3V引脚同时供电,并且一直供电?

(2)我想打开第一个开关管,采用的程序执行流程是:1.使得EMB1428片选信号为低;2.发送关闭所有开关管的命令;3.将片选信号置高;4.延时1s;5.使得EMB1428片选信号为低;6.发送打开1号开关管的命令;7.将片选信号置高;8.延时1s

但是返回的数据是0x90和0x91,也就是错误代码是1001,请问这是什么原因?该如何修改错误?

  • 把电路图发上来看看?

  • 原理图在下面,这是一部分

    EN和DONE,以及DIR和/DIR之间通过反相器连接

    只用来控制5节电池的开关矩阵,所以中间两个开关的驱动输出引脚直接拉低了

  • 今天实验发现新问题;

    (1)如果在循环里重复切换开关1和开关2,每条指令间隔时间设置为5ms,具体流程如下:1.使得EMB1428片选信号为低,延时5ms;2.发送打开1号开关管的命令,延时5ms;3.将片选信号置高,延时5ms;4.使得EMB1428片选信号为低,延时5ms;5.发送打开2号开关管的命令,延时5ms;6.将片选信号置高,延时5ms。

    这时发现返回的数据还是0x90和0x91。

    但是如果循环里只有打开一个开关管的命令,是可以成功返回正确数据的,但是EMB1428的驱动输出引脚没有电压(此时开关管没有焊接,仅仅测试输出引脚电平)。

    (2)测试发现CEXT1和CEXT2引脚有1MHZ的方波输出,幅值大概是12V左右,请问是不是只要有方波输出就可以产生开关管驱动电压了?但是在仅打开一个开关管的实验中,并没有在EMB1428的输出引脚检测到驱动电压。

    (3)手册中有说明在执行新指令的时候,会将EN引脚先置低再置高,请问新命令是不是指打开一个不同的开关管,如果重复打开同一个开关管,是不是认为这不是一个新命令,从而EN引脚电平不发生变化?

  • 在EN和DONE的反相处理时,有没有加延时?即EN信号有效一段时间后,DONE信号才有效。

  • EN和DONE之间用的是反相器,器件型号是TI的SN74LVC2G14-Q1

    刚才做实验发现带开关管做实验时,如果循环里只有接通第一节电池的命令,可以成功打开开关管,但是如果程序里循环切换连接不同的电池(比如循环切换1号电池和2号电池),返回的数据还是0x91和0x92

  • 补充说一句,我做实验的时候,没有接电池,仅仅只是焊接了开关管,这会对实验有影响吗?