使用TPS40428+2*CSD95378来提供核压电源,CSD95378需要5V供电,单板没有5V电压,能否使用TPS40428的BP5来给两片CSD95378提供VDD电源?我看电压范围是可以满足的,CSD95378所需电流没有找到,谢谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
使用TPS40428+2*CSD95378来提供核压电源,CSD95378需要5V供电,单板没有5V电压,能否使用TPS40428的BP5来给两片CSD95378提供VDD电源?我看电压范围是可以满足的,CSD95378所需电流没有找到,谢谢!
Hi
TPS40428的BP输出总带载能力在40mA左右,而单片CSD95378 VDD的电流在频率500kHZ时就是27mA左右,不足以带动2片。
需要用其他电压搭个5V出来,电流能力不要设置太小。