请问:
如上图所示,为什么TPS65000热阻Rja,同一个芯片,相差很大(270‘C/W 和48.7’C/W)?Power rating是什么含义?谢谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
这两个参数的测试条件不一样,如下面(1)和(2)所描述的,(1)使用的是两层析,2盎司的铜箔厚度的布线下测量到的,(2)在多层板,1盎司的铜箔厚度布线下测量到的。
网上有一篇文章供参考:www.21ic.com/.../123074.htm
power rating是指在所指的条件下耗散相应的功率后温度升高1摄氏度。
Hi:
芯片利用其Powerpad与PCB 大面积的GND铜箔充分焊接,将GND铜箔当做散热片,所以不同的PCB(1s ,2s2p),散热效果会非常不同。
Power rating 是在该条件下的芯片的最大功耗,例如RqJA =270°C/W 热阻条件下,环境温度是70℃,最大芯片功耗是204mW, 此时芯片温度是70+270*204/1000=125℃, 即芯片最高结温:Maximum junction temperature, 125℃ ,也就是说最高结温和热阻将决定不同温度下,芯片的最大功耗。