This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
有测试CS等脚的波形吗?
谢谢回复!
Cs波形我测了一下,是还算标准的三角波,没有发现什么异常,我怀疑这个台阶是米勒电容引起的,因为我现在用的MOS是STF18NM80,Qgd是40nc(Vdd=640V,Id=17A,Vgs=10V),我是参考设计TIDA-00701,我买了一些参考设计上用的AOTF15S65L,Qgd是5.6nc(Vgs=10V,Vds=480V,Id=7.5A),回来测试一下,看一下比较结果。
亲;确实是米勒效应所至。管子用的太大了。建议换600V或650V管子试试。
你做多大功率电源用这么大的MOs管?
做100W左右,工业应用,我主要想减小温升,留的裕量比较大。
改用650V耐压的mos管,修改了一下RCD吸收电路,改小电阻,加大电容,TVS限压180V,RC电压限制在175V左右,TVS主要过滤掉尖峰。
看起来确实像是Qgd偏大,也就是米勒效应导致的
25mA的驱动电流,确实小啊