Other Parts Discussed in Thread: TPS65262
TPS65262规格书里,对3个buck的EN脚高低电平说明是:
高电平1.2v~1.26v,低电平1.1~1.15v。
首先高低电平太接近了,1.2v和1.15v只差了0.05v,这太难保证了。另外高电平为什么要有max值1.26v,低电平为什么要有min值1.1v呢,不是应该反过来,高电平有min,低电平有max吗?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
高电平电压建议高于1.26V, 例如3.3V
低电平电压低于1.1V, 例如0V.
高电平1.2v~1.26v,低电平1.1~1.15v。其中1.2V和1.15V是典型值,1.26V是最大值,1.1 V是最小值,这是符合高斯分布的。
换句话说大部分芯片在高于1.2V时芯片启动,低于1.15V时关断,小部分要高于1.26才能打开,低于1.1V才能关断
VCC是V7V,MODE是单独的mode管脚
你要先将EN3接地,然后上电,最后上电EN3。具体可以参看数据手册的图26
你的方式还是要先将EN3拉至GND,然后拉高才能实现你的功能