Other Parts Discussed in Thread: TPS61088
效率高达 91%(VIN = 3.3V、VOUT = 9V 且 IOUT = 3A 时)
这是datasheet上写的。
我给并联18650锂电池升压,VIN = 2.8V-4.2V,
如果VOUT改为6V,IOUT=3A,效率是不就会低很多?
如果VOUT还是9V,IOUT=3A,因为输入电压范围变了,效率是否也会降低?
我想了解给3节18650锂电池并联升压,升到几伏几安输出效率最高?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: TPS61088
效率高达 91%(VIN = 3.3V、VOUT = 9V 且 IOUT = 3A 时)
这是datasheet上写的。
我给并联18650锂电池升压,VIN = 2.8V-4.2V,
如果VOUT改为6V,IOUT=3A,效率是不就会低很多?
如果VOUT还是9V,IOUT=3A,因为输入电压范围变了,效率是否也会降低?
我想了解给3节18650锂电池并联升压,升到几伏几安输出效率最高?
Hi
输出主要看你的输出电压要求,如果你的输出电压可以是6~9V, 6V满载效率会高一些。
关于转换的效率,你也可以用webench确认。(你可以看一下效率曲线)
Johnsin Tao您好
上面帖子我有个地方写的对不,负载工作功率是13.5W,我这边没有61088,用电源箱模拟了一下,设定在9V2A或者6V3A的条件下,都可以让负载正常工作,实际消耗是9V1.5A,或者6V2.25A,13.5W。所以TPS61088可以输出9V2A或者6V3A,TPS61088的供电是3节并联的18650电池,这两个输出,哪个效率更高呢?
Hi
9V/1.5A 与6V/2.25A效率差不多,前者在92%左右,后者93%左右。具体取决于你的电路设计,包括电感。从效率波形上看峰值效率并不是在3A时,而是在中间靠后的位置。
你可以借助webench仿真确认,输入设置3~4.2, 输出设置9V/3A, 6V/3A.
效率不仅取决于开关损耗,还取决于电感电容上的损耗,还和你的layout相关(散热),所以最好你先用WEBENCH或Tina进行仿真验证,再参考推荐电路以及PCB进行设计