使用LM3401设计了一个4.5-35V输入的LED恒流驱动电源,但是在实际测试的时候,5.5-6.5V时,电流波动明显,输出电流能达到1.5A,正常的恒流设计是1A。请大佬指点一下,是设计上的问题吗?一下是原理图。其他电压范围都是OK的,调节电源恒流1A输出,就是在5.5-6.5之间会出现一段1.5A输出的情况,测试IC输出波形很乱,其他情况下是好的。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
输出不建议用1000uF这么大,建议1uF左右陶瓷电容。
其次请问你的LED灯电压是多少(VF)?