Other Parts Discussed in Thread: BQ25890, BQ25892, PMP40060, BQ25895
1、采取BQ25890,USB BC1.2只到5V,1.5A。如何判断为DCP?调节USB的D+/D–,是由adapter端输出D+/D–,与BQ25890的D+/D–连接,判断为DCP,再通过Current Pulse Control Protocol来控制VBUS?VBUS电压调高是如何实现的?OTG功能理解为:HOST可以输出OTG为高,OTG_CONFIG bit=1,可以使能boost mode,,由BAT升压从VBUS输出5V,2A到给外部设备供电?
2、BQ25892如何接PSEL,从而判断是USB SDP还是Adapter? PSEL由主控来判断?BQ25892充电电流只能设置为500mA或3.25A两种,那输入电压也是通过Current Pulse Control Protocol从而调高VBUS电压? PSEL只能区分USB host和adapter source类型。
3、我们AC/DC部分,采取PMP40060+PMP40133的解决方案。PMP40133的MSP430G2955IRHA40R软件部分需要自己开发?该方案用普通USB-B的connector就行?如果向下兼容QC2.0,是否可以直接用符合QC2.0的充电器就行?