This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

我的BQ2057C充电截止电压为什么是4.1V?

Other Parts Discussed in Thread: BQ2057C

我用BQ2057C做的充电管理,电路图是手册里面的图,用的MOSFET,为什么电池冲到4.1V就停止了,充电状态就变了?

  • 有以下几点建议供参考

    1;确认芯片是CV电压为4.2V的BQ2057C,而不是CV电压为4.1V的BQ2057

    2;请启用芯片的自动补偿功能,如果之前的电路中就有启用但收效甚微,建议可以适当将补偿值放稍大一些。(非常关键,BQ2057C芯片设计这个功能就是为了避免遇到因为layout 的影响而使得电池不能冲饱)

    3;我们知道芯片进行充电截止的判断标准是检测SNS电阻两端的电压差(参考电压点在高端时为Vcc,在低端检测时为GND ),当SNS电阻两端的电压低于我们datasheet中给出的电压门限值时就会判断已经充饱,所以如果我们选择了某一个SNS电阻的情况下,比如电流小于20mA时,两端的端口电压刚好降低到iterm门限,但我们如果选择更大一些的SNS电阻,则20mA时,两端的电压差还是大于iterm门限从而使得充电能继续进行,也意味着可以让电池端口电压再上升一会,当然这个更好的充电效果是以减小CC模式下的充电电流为代价的,这意味着整体的充电时间将会比之前要长。

  • 你好,怎么样才能增大补偿值???CC与COMP引脚的具体的作用什么???CC是怎样实现驱动功率管的???COMP是怎样实现动态补偿的呢????

    非常感谢您的回答!!!