This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC28600不能正常启动



用过28600的大侠给支一招吧,我照着PDF资料上给的电路画原理图和PCB,现在的现象是这样的,输入端从0----80V时,电路一直在打嗝启动,输入端的电压加到AC100V时,启动终止,测得VDD端的电压是12.8V---8V之间,输出电压是6---7V,实际设置的是27V,VSS端的电压用示波器观察到1.2V就关断了,然后就再也不会启动了,VFB脚为低,VDD上升到12.8V时,VFB出现一个4.2V的脉冲,整个过程中7脚电压期为0,3脚的电流峰值为500 mA 。启动电阻3.3M,启动电容22UF,变比初级:次级:反馈是90:12:6,初级电感量530 uH ,变压器AE=118;1脚电容为223;2脚电容为331;3脚电容为471;5脚驱动电阻为10;7脚上偏电阻为80K,下偏电阻为24.9K。

帮帮忙,着急!!!跪谢!!!