电源电压3.6V,需要±12v输出,输出电流可以达到100mA,LT1054是不是不能由3.6转为12V啊
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
电源电压3.6V,需要±12v输出,输出电流可以达到100mA,LT1054是不是不能由3.6转为12V啊
Hi
是的, -12V就是+12的反向。
这个设计是输出+/-15V, 30mA是负载电流,这个电流可以做大一些,但是需要选择TPS61081.
再问一下,TPS61080最大不是可以输出500mA么,chargepum电容是指C3是吗,谢谢
Hi
500mA是开关电流, 在升压转换中,这个电流时输入平均电流加上二分之一的电感纹波电流(500mA>= 输入电流Iin+ 纹波电流/2)。通过功率转换可以评估最大输出电流。
例如假设纹波电流时输入电流的0.3倍,效率是85%, 那么根据 输入电压Vin* 输入电流Iin* 效率= 输出电压Vo*输出电流Io, 所以最大Io= Vin * 500mA/1.1*0.85/Vo
chargepump电容是指C2
你好
使用TPS61081进行测试,+12v输出正常,-12v输出只有-1.27,L和SW电压为3.3V,FB端输出1.3V正常,均未接负载,请问是什么原因呢
Hi
检查的D1/D2的焊接,包括看是否有反向。
你好
仔细检查电路连接正确,二级管没有接反,二级管使用的是IN5819