This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

tps65217配合Am335x处理器,由于外部电源不稳造成锁死问题

Other Parts Discussed in Thread: TPS65217

采用tps65217和am335配合的核心板,供电电压是5V    ,由单节锂离子电池(3.6-4.2V)升压和外部适配器12V降压得来。

当外部市电断电以后自动切换到内部锂离子电池供电,当锂电池电压降低到3V左右时,电池电压不稳定,电池保护,造成升压的5V也不稳定系统无法启动,然后电池电压会恢复到3.2V左右,5V供电稳定了,但是系统还是锁死。  甚至外部市电恢复供电也无法恢复系统。

请问下有遇到这种情况的吗?