用BQ76940设计了一个电池采样电路,测试发现了一个疑问,B5和B10两个地方耗电不一样,按照BQ系列芯片设计,每5串为一组,B5和B10的耗电应该是接近一致才对,而实际测得是B5最大17.8uA,B10最大5.6uA,那么请问这个是否正常。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
用BQ76940设计了一个电池采样电路,测试发现了一个疑问,B5和B10两个地方耗电不一样,按照BQ系列芯片设计,每5串为一组,B5和B10的耗电应该是接近一致才对,而实际测得是B5最大17.8uA,B10最大5.6uA,那么请问这个是否正常。
附件是我这边的图纸,您的意思是说,B5多出来的功耗是控制那个到REGSRC的MOS管基极引起的,但是不会多出这么多吧
那个还有有的,另外,你这M12的基极和VC5X之间需要个电阻,100K,这个MOS是工作在线性区的,并且最好串个分压电阻和二极管,
R114, R120 , R127 选择1K,
C40, C42, C57 选择10uF,