This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC28019A电流采样问题

Other Parts Discussed in Thread: UCC28019A, UC2844, UC2854

UCC28019A电流采样可以像UC2844那样采样吗?

  • 你好,

    UCC28019A是PFC控制器而UC2844是桥式PWM控制器,后者一般在MOSFET源极和地之间串联一采样电阻进行电流采样,而前者采集电感电流,芯片里面是要计算平均电流的,所以采样电路应该串联在主回路里。

    希望可以帮助到你,谢谢。

  • Hi

         两个控制芯片topy都不一样,控制方式都不一样,建议按照芯片datasheet具体说明具体设计。

  • 你说的跟2844那样采样时什么意思?从原理上来说,28019A的电流i采样跟2844的采样是一样的,都是在功率回路串联一个取样电阻。唯一的区别在于,2844电流信号需要的是一个正值,28019A需要的是一个负值,所以IC接地的位置有所区别而已。

  • 你好,

    根据手册推荐的应用电路,UC2844的采样电阻和MOSFET串联,因此只需要采集电感上升电流波形即可。而UCC28019A采样电阻采的是电感电流,包括电流的上升和下降,手册18页中提到采样的电流会内部放大器做平均计算,之后利用ICOMP脚电容做补偿。因此建议采用手册上的电路进行电流采样。

    希望可以帮助到你,谢谢。

  • 你好,

    平均电流单周期控制,你要对比的应该是UC2854