Other Parts Discussed in Thread: TPS62130
tps62130在使用中,无输出了,设备拿回来打开检查后,发现无输出,芯片发烫,这有可能是什么原因?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: TPS62130
tps62130在使用中,无输出了,设备拿回来打开检查后,发现无输出,芯片发烫,这有可能是什么原因?
HI
请问在使用中你是多少输入,多少输出(只要是电流电压)?
设备拆开后,断电测试芯片,PVIN, SW脚对地阻抗如何? PVIN与 SW 的阻抗如何? (确认是否有击穿导致的低阻抗)
不良率多少?
15V输入,3.3输出,没有感觉mos管被烧坏,PG脚上电就接地,没有负载情况下,静态电流6mA
Hi
如果这类不良比较多,你可以更换芯片来确认是芯片坏掉了。
如果通过阻抗确认MOS没有损坏,而芯片只是漏电流比较大(静态电流太大),可能是Vin输入过压导致的损坏。
输入15V距离规格上限比较近,如果输入有较长导线,或者输入走线不好,输入容易因为寄生电感造成较大spike, 叠加到输入就会过压。
(如果输入有导线,建议在输入导线接线处增加一个较大电容如100uF。另外芯片输入走线尽量宽一点,输入电容尽量靠近芯片Vin脚)