Other Parts Discussed in Thread: UCC28700, UC2844, TL431, UCC28740
请帮忙推荐几款内置高压启动的电源管理芯片,谢谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
TI的UCC287XX系列,见:http://www.ti.com.cn/product/cn/UCC28700 等
UC28700规格书上写的是原边电压反馈,了解一下一般用于手机充电器精度为5%;
我现在用的是UC2844,通次级通过线性光耦+TL431反馈,精度为1%,但是静态功耗太大
请问UC28700可以用于次级线性光耦+TL431反馈吗,或者其他芯片也可以,谢谢
Hi
这个系列的芯片中例如UCC28740: http://www.ti.com.cn/cn/lit/ds/symlink/ucc28740.pdf
这些芯片就是用光耦+431做反馈的。
这款28740看规格书是用在消费类和白色家电行业,可以用在DC-DC、变频器、UPS等工业领域吗?
这款芯片驱动功率太小了,25mA,推荐一款驱动功率大一点的芯片
看推荐设计文档,最大交流输入是264A,应该是AC220V电压等级的,我现在应用是AC380V电压等级的
| Maximum Input Voltage, VINPUTmax = | 264 | VAC |
你的电源输出功率是多少?UCC28740做到大几十瓦没问题。
我这边需要做到一百多瓦,有没有输出峰值电流1A左右的同类型电源芯片