This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

关于TPS61196最小电流

Other Parts Discussed in Thread: TPS61196

The TPS61196 provides a highly integrated solution for LCD TV backlight with an independent PWM dimming
function for each string. This device is a current mode boost controller driving up to six WLED strings with
multiple LEDs in series. Each string has an independent current regulator providing a LED current adjustable
from 50 mA to 400 mA within ±1.5% matching accuracy. The minimal voltage at the current sink is
programmable in the range of 0.3 V to 1 V to fit with different LED current settings. The input voltage range for
the device is from 8 V to 30 V.

数据表上有这么一段,TPS61196最小只能50mA吗?还是通过ISET设置最低只能50mA?如果采用PWM控制能不能做到更低?