电源输入24V,LED为 10 × 4个LED , 4个一组串联,共十组(见图1);
用的是cree的5MM灯珠,压降在3.2V左右 ,作电流为20MA。(参数见下图2)
要求可以通过输入一个模拟调节去控制LED阵列亮度,调节范围为0 --- 30MA
图1
图2
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
采用多路控制,一般是升压来做,类似TPS61195,LP8555之类。
如果你是降压,或可以将10串并联来做做看,选择LM3402之类降压的芯片。
这个我也正在选型,有没有多通道RGB 调光的IC.
这种升压或者降压的芯片有较上面的有什么优势和区别吗
我想问问采用多路控制,是否有通过电位计实现模拟调节功能的芯片呢,我看TPS61195只有PWM和SMBUS两种调节方式,