This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ24650充电自动停止问题



充电模块原理图如下,各关键点测试电压为:Vmppset=1.32V ,Vvcc=18.49V,VSRN=13.39V,Vregn=6V ,VREF=3.3V,VFB=1.39V,通过公式计算,充电电流应该为1A,          但实际的充电电流只有100mA 左右,并且在充电一短时间后充电停止,此时测量上述关键点电压不变,VCC重新上电后,充电电流恢复100mA。

 充电电池磷酸铁锂电池和铅酸电池都试过,同样的现象。