电池是单节或多节并联锂电池,容量4000mAh左右。
项目方案要求电源是5V供电,最大能提供2A左右电流。
1、最好是单芯片方案,无需外部MCU参与控制,兼顾有充电LED状态指示。
2、拥有过充、过放、防倒灌、放反接、过压、欠压等保护电路。
3、拥有电源路径管理功能,即接外部电源时既能给电池充电,又能给其它外围电路供电;不接外部电源时,由锂电池给其它外围电路供电。
4、外部充电接口采用的是Micro_USB口,5V电源输入,最好可以不使用D+和D-线检测。
5、充电电流能达到2A左右。
6、若集成电量指示最好。