一直在用TI的评估板BOOSTXL-DRV8305EVM。
Supports 4.4- to 45-V voltage supply and up to 15-A RMS (20-A peak) drive current
上面用到了LMR16006。
原理图如下:
但是按照16006手册中我计算了一下。
最大输入电压按45V,输出3.3V,Io =0.6A,Kind = 40%, 开关频率 = 700K.
计算求得最小电感也要18uH.但是这里选择了一个15uH 的电感。
这是怎么一回事那?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
一直在用TI的评估板BOOSTXL-DRV8305EVM。
Supports 4.4- to 45-V voltage supply and up to 15-A RMS (20-A peak) drive current
上面用到了LMR16006。
原理图如下:
但是按照16006手册中我计算了一下。
最大输入电压按45V,输出3.3V,Io =0.6A,Kind = 40%, 开关频率 = 700K.
计算求得最小电感也要18uH.但是这里选择了一个15uH 的电感。
这是怎么一回事那?
HI
纹波电流选择为输出电流的0.2~0.4倍 按照你选择0.4也行。
实际应用中的电感感量与计算出来的感量接近就可以。(电感厂商只提供常见常用感量的电感,15uH很常用,如果有18uH,你也可以选用。如果运气不好算出来时16.5uH, 选择15uH/18uH都可以)。
感量略有偏差,只会造成满载时纹波电流的差异,只要 纹波电流分布输出电流的0.2~0.4倍附近就可以。 试想假设你工作在非满载状态时,按照当时的电流来算,计算得到的感值肯定也不会是你用的电感感值。
电感饱和电流一般推荐选择为最大输出电流的1.2倍以上,留一点余量。
你好,
电感电流纹波系数不一定非要在0.4以内,只要在附近就可以,还是要按照具体情况来看。这块EVM上降压部分看起来布局空间较小,而电感体积相对较大,因此可以适当提高纹波系数,只要保证电路在一定范围内仍可正常工作即可。
A reasonable value is setting the ripple current to be 30%-40% of the DC output current.
手册中写的30%-40%,和您说的差不多。
明白了很多。
TI的datasheet写的真的非常好。
谢谢。