用了TPS62745DSSR将9V的方块电池降压到3.3V,想知道该芯片能否进行低电压检测,需要在9V方块电池低于8V时有个变化的信号可以检测。芯片的PG引脚好像可以检测转压后的电压,如果输出小于阈值电压(2.9V)就会翻转。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
用了TPS62745DSSR将9V的方块电池降压到3.3V,想知道该芯片能否进行低电压检测,需要在9V方块电池低于8V时有个变化的信号可以检测。芯片的PG引脚好像可以检测转压后的电压,如果输出小于阈值电压(2.9V)就会翻转。
Hi
不能用到芯片的欠压保护,原因是当输入降到3.3V以下,早已不能维持3.3V输出了。
如果需要做欠压保护,需要额外的芯片来做。
你好,我外部电压最低差不多8V就没法用了,这个8V电压有什么额外的芯片可以检测出来的,要低功耗的。
你是希望电池在8V时,仍有输出,只是发送一个检测信号给后端么?
其实你可以在输入加分压电阻,后端单片机直接读取或者 分压后的输入电压加比较器输出检测信号
当然。
你可以选择大电阻,这样功耗就会小一点
这样也可以,R9改小一点50ohm以下,这样电路反应会快点,检测的准确度也会高点
3.3V MCU的引脚能否直接驱动N-MOS管,例如AO3400
有个问题要注意一下,这个用于高端电压控制的mos管应该用PMOS,S接9V,D接R4.
实际上这就是该芯片提供的一个功能,VIN_SW输出脚就接分压电阻送入MCU的ADC就可以了,MCU控制EN_VIN_SW在不检测电压时切断这个输出电压来实现低功耗。