This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS7A3301使用过程中出现奇怪现象

Other Parts Discussed in Thread: REF3220

 芯片:TPS7A3301;

LDO:-18V转-15V;

芯片工作模式:Adjustable Operation;

所使用的adjustbable电阻都是芯片手册中推荐的值。

结果:上电后用万用表测量芯片输出,输出的值是-17V左右,但是不稳定,会慢慢的以0.01V下降,等了一段时间后,再次测量,这时电压已经降到-16.4V左右,基本上就稳定在-16.3V左右吧。

问题排查:我测了其他板子上的芯片也是这样的问题,虽然换了芯片,也更换了电阻,但现象并没有改善。等再次上电时测量,电压就基本上是-16.3V左右吧,但不会在-15V左右。我所使用的电阻值都是手册推荐的。不知道这是为什么?

2、还使用了一个TPS7A4701,是18V转15V,也是使用的手册推荐阻值,它的输出就很正常,在14.7V。