用TPS51200产生VTT作为DDR3地址和控制线的端接电源,不知该怎么估算其消耗的电流,请TI的工程师帮忙解答
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
不太明白你的意思,你的打算算负载端的消耗吗?对于这类芯片而言,直接测试即可。对于负载端,一般电流需求也是有规格的,在3A内即可。
而且系统电流的需求也是变化的: Because the device does not sink and source current at the same time and the I/O current may vary rapidly with time, the actual power dissipation should be the time average of the above dissipations over the thermal relaxation duration of the system.
你好,情况是这样的:
TPS51200是从系统的3.3V取电,因为同时还要带其他负载,我需要知道3.3V电源会被51200取走多少电流,最终的目的是确保3.3V电源有足够的输出能力。
Hi
由负载端决定,你需要确认负载端最大电流需求。对于TPS51200, 负载端电流需求也就是输入电流需求,这个没法算的。