请教下LM2940C手册上**COUT must be at least 22 μF to maintain stability. 这个电容有点大,没有小封装尺寸的。能否在输入0.1uF,输出10uF和0.1uF。采用常规三端稳压采用的配置电容。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
如你所提到,这个LDO是需要在输出至少22uF电容才能稳定。
你或可以采用2个10uF电容看一下效果,是否满足你的需求,不建议只用一个10uF。
或者你重新选择一款LDO,很多LDO并不需要这么大的输出电容的。需要指出的是LDO在输出电流较大的情况下,输入输出压差不能太大,否则功耗很大,效率很低。
你可以看一下TPS73801之类。
这个你需要在LDO List中慢慢找: http://www.ti.com.cn/zh-cn/power-management/linear-regulators-ldo/single-channel-ldo/products.html#p451max=0.9;1.1
你可以多设置一些条件,例如输出电流在0.9~1.1A, 输入电压范围,封装等之类,这个可以缩小范围。 然后再在合适的芯片中通过datasheet来确认输出电容的需求。