Other Parts Discussed in Thread: TPS61040
TI工程师,你好。看资料写此芯片的是最大能升压到500V,最大提供10mA电流。不知道是否理解为提供5W功率,350V应该最大能提供14mA的电流。这么理解对吗?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: TPS61040
TI工程师,你好。看资料写此芯片的是最大能升压到500V,最大提供10mA电流。不知道是否理解为提供5W功率,350V应该最大能提供14mA的电流。这么理解对吗?
Hi
不要这样理解。
最大升压和功率没有明确的相关性,但是当输出电压非常高时,一般设计电流会相对较小。而当输出电压不高时,电流可以很大,并没有5W的限制。
请问你具体要做多少输入,多少输出的电源转换?
你好,很高兴看到你的回复。刚画好图了,我是要利用这个芯片,把输入9V的电压升到260伏来用,要求电流很低,mA级别。电路已经画好,但是在手册中没说明Cout如何选择计算,在手册的事例图中(手册第18页,8.2.1,Figure30)是把3.3升到5伏使用,选用的充电电容电容(Cout)为10V,100uF。我升到200多使用,电压高了,很难选到这么大容量的电容,不知道这个电容应该如何选择?