This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

想要使用12V降压到5V,电流大概150mA.使用TPS7A4501可以吗

Other Parts Discussed in Thread: TPS62175, TPS560200

想要使用12V降压到5V,电流大概150mA.使用TPS7A4501可以吗?

不晓得发热大不大,求解

  • Hi
    如果不介意其效率只有40%左右,用这个芯片是可以的,因为功耗只有1W左右,而这个芯片热阻并不高。
    这类LDO的优势是纹波noise都很小,如果在意效率,建议选择DC/DC,例如TPS560200,TPS62175都是可以的。