This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM1117-1.8电源芯片,工作一会后,输出正负极间的电阻很小,近视短路

自己参照开发板做了一个DSP28335的板子,电源芯片是用的ASM1117-3.3和LM1117-1.8,上电初期,程序可以下载,并能正常运行。几分钟后,电源芯片温度上升至32度左右,程序跑飞,然后DSP芯片冒烟烧毁,检测电路发现是电源正负极短路。测了电源芯片输出电阻,1.8V的芯片只有几欧姆,等时间过久一点,芯片温度完全降至室温26度时,电源输出电阻为200欧姆。然后再换了一片DSP芯片后,板子其他地方不改动,通电后,又能正常工作,工作一会后,程序又跑飞,断电测电阻,又几乎是短路了,,,,

  • Hi

        LDO的输入电压是多少?而正常带载1.8V,和3.3V的电流分别是多少?(我需要确认功耗和是否有过压风险)

        LDO在使用条件上如果功耗偏大是容易造成芯片温度偏高,但是只是32℃,代表功耗很低,你是如何得知芯片温度的?

        对于LDO,如果输入输出短路,断电后并不会恢复(烧掉就是烧掉,不会再好的)

        一般这类芯片,如果功耗很大,会过温保护如shutdown.

        另外你的芯片哪里买的?  

  • 芯片最高温度可以到125度,你DSP烧毁,是因为大电流么?

    芯片采购渠道正规么?淘宝上几乎都是假货。建议官网申请样片。