1. 我准备采用12V电源接入,通过升压芯片LM3478到16.8V,给充电芯片BQ24610。但是在测试LM3478的过程中,我需要的电流为3A,但是发现LM3478在2A时就自我保护,开始跌落,请问这是什么原因?
2. 我准备做一款便携式产品,之前是24V降压到12V方案,但是发现MOSFET发热严重,所以后来准备改由12V接入,采取升压方案,是否有其他更换的芯片推荐,可以完成我的整个电路?
谢谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.