我想问一下,如果用tpS76850从7.2V电压稳到5.0V,它的外围电路7(FB/NC)和8(PG)引脚是不是不用接器件,直接悬空就可以?或者是?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
tps768xx功能电源良好(PG)输出,可用于监测监管的现状。这个内部比较器监视输出电压:当输出降至标称值的92%和98%之间时。调节值,PG输出晶体管接通,接收信号低。开漏输出需要一个上拉电阻。如果不使用,它可以悬空。PG可用于驱动上电复位电路或用作低电量指示器。当规定的输出电压下降到指定的2%时,PG不会断言。容差,而是报告输出电压低,相对于它的标称调节值。调节器保护tps768xx PMOS晶体管的内置了一个反向二极管进行反向电流,当输入电压低于输出电压(例如,在断电时)。电流从输出到输入并不是内部限制的。当预期延长反向电压时,外部限制可能是。的tps768xx还具有内部电流限制和热保护。在正常操作期间,tps768xx限制输出电流约为1.7 A时,输出电压与电流限制,尺度线性恢复,直到过流状态结束。虽然电流限制是为了防止总装置故障时,应注意不要超过包的额定功耗等级。如果温度该设备超过150°C(典型值),热保护电路关闭它。一旦设备冷却到下面130°C(典型值),稳压器操作恢复。