This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Bq24160的一些问题求助



背景:以前手边的Li电池管理都是用ATMEL406作的,不合适作单cell的管理,因此选择bq2416x或者bq2418x来作。

第一次用这个片子,希望能得到些指导:

1.内部寄存器的地址.In databook(http://www.ti.com/lit/gpn/bq24160), "The device 7-bit address is defined as ‘1101011’ (6Bh)." 它没具体告诉每个寄存器的地址,如果我通过I2C怎么访问?

2.没找到软件的一个流程图,就是叫我先配哪个寄存器,再配置哪个寄存器,另外比如我更新了寄存器的参数,如何让新参数生效,这些新参数是掉电保存的吗? 

3.In databook(http://www.ti.com/lit/gpn/bq24160), Fig3 提出 GSM的功放 直接连接到电源上.在这个操作下,功放是一直工作的,而且PA的供电没有经过整流,这样作没有问题?另外是否是符合阈值电压的PMOS可以直接连接到BGATE,不需要下拉吗?

4.手册上的Fig1.上的QFN的16Pin是SGND,后面的Pin description没有提,想问下如何处理它.