This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS65270带载增加后,输出电压降低的厉害



我的设计为12V输入,3.3V,4.2V输出,现在测3.3V的时候,发现带载能力不够,负载电流大了以后,电压就降低了,以下时我的测试数据和电路图。

lx波形图

当我把R39换成0R的时候,在输出1a的时候,电压下降到了2.580V,lx波形图如下:

针对这种带载能力不够的情况,我要增加电感感量吗?或者有没有其它建议?