我把TPS54260的反馈接到了LED上面,这样就可以横流输出了.但现在的问题是,发现电流不够 ,可以用两个并联吗?一起做横流输出.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Yang,
Yes,Theoretically you can operate with two TPS54260 in parallel. Yo will need to be careful not to operate in eco-mode. Eco-mode operation is difficult to predict. If one device is in eco-mode and the other is not you may not share current equally. That being said, you may not care about absolute current sharing at very light load. The main issue is at higher loads where one device may be driven to current limit while the other is in light load operation. Making the COMP pins commom will insure the two devices share current equally in CCM operation but in DCM and especially eco-mode they may not share well.
Hi :
两个TPS54260直接并联会出现功率平衡的问题,需要均流,否则容易出现其中1路电流过大,而另一路电流非常小的问题,虽然会电流保护,但也因此会出现不稳定。
如果你一定要使用TPS54260, 就需要尝试外部加CLK信号,同步2个芯片,见datasheet :http://www.ti.com.cn/cn/lit/ds/symlink/tps54260.pdf 第二十二页。
Hi
或许你可以选择LM3409: http://www.ti.com.cn/cn/lit/ds/symlink/lm3409.pdf 这样大功率LED驱动的芯片设计。