This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ25895输出电压不稳

Other Parts Discussed in Thread: BQ25895

BQ25895,在不接电池的情况下开机会出现重启,测试输出电压发现有瞬间掉电现象,帮忙分析可能是什么原因?

电路图如下

  • Hi

    电池充电时恒流设计,测试时需要接负载电池,不然怎么恒流?

    在你的电路中,输入给5V, 经过D12后只有4.3V左右,而电池电压如果要充满大约是4.2V, 这之间的压差比较小,建议提高一些输入电压。

    BAT输出给电池充电,需要并联一个10uF电容。

    轻载上述修正后再测试,看看是否仍然有问题?