This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

我想问,TI的 WEBENCH推荐的设计原理图是否靠谱???

我按照推荐的设计原理图画板,现在在调试,发现一直启动不了,初步确定是反馈绕组无法提供芯片后续的供电。

(问题1):按照我的输入范围是: DC20-280V输入,TI推荐设计的原理图启动电阻是两个2.49K/0.25W串联,那如果输入280V,在这两个电阻上面功率不是超大?不会烧毁吗?

(问题2):在20V输入的时候,能不能通过其他方式,提高启动电阻的阻值,降低功率?

 附件是我的原理图,麻烦路过的大神帮忙看下,点评一下。指出哪里的不足之处。谢谢各位!DC20V-280V电源模块.pdf

  • Hi
    就经验看是非常靠谱的,但是对于隔离芯片的电路设计,因为牵涉变压器,仍建议你自己计算确认一下。
    目前测试情况显示是二次供电不足吗? 如果再供电绕组增加1~2圈呢(实际算一下)?
  • 您好,目前测试,我使用20K的启动电阻,发现要到260V左右芯片才能正常工作,不然就是一个三角波,量了一下辅助绕组输出,电压只去到4V左右,偶尔有一两个尖峰去到8V,增加辅助绕组匝数能使芯片启动吗?