This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

咨询bq2060问题

Other Parts Discussed in Thread: BQ2060

您好:

    我在使用bq2060的时候,选用了20m欧姆的采样电阻(确定是20m欧姆电阻,不是10m欧姆电阻)
    故设置
      ADC Sense Resistor Gain = (u16)(625.0 / 0.020);
      VFC Sense Resistor Gain = (u16)(409.6 / 0.020);
    因为手头上的工具不全,未做电流、电压和温度校正
    但遇到了问题

    我使用负载仪放电,放电电流为3A,但bq2060检测出的放电电流仅为1.5A
    使用充电器充电,充电电流为5A时,bq2060检测出的充电电流为2A;充电电流为4A时,bq2060检测出的充电电流为1.5A

    该怎样解释这种情况了,未做校正也不至于相差这么大吧?

----------------------------------------------------------------------------------------
    bq2060的充放电电流采样的时间间隔是多少?如果充放电频繁是否会造成测量误差?我在手册上看到使用了ADC来检测电压、温度和电流,使用VFC来检测充放电电流,这里检测的两个电流有什么区别呢?

----------------------------------------------------------------------------------------
    还有,能介绍下使用了bq2060的电池组的装配过程,从全新未充电的电芯,组装最后到出厂的过程,谢谢了