Other Parts Discussed in Thread: UCD3138A, UCD3138
UCD3138A的datasheet中,24-bit PWM Timer和16-bit PWM Timer的时钟都是Interface Clock,但是这个Interface Clock时钟频率到底是多少啊?Datasheet中好像找不到!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
HI
应该是通过程序寄存器中获得。建议你通过找授权代理商拿到历程来确认,这个应该是要签保密协议才能获得的。
你好,
在文档 UCD3138 Technical Reference Manual中第379页,11.2中有以下描述
The core of the T24 timer is a 24 bit free-running counter. The clock input for the T24 timer can come from a clock within the UCD3138, ICLK, which is nominally 15.6 MHz.
你可以在以下链接下载该文档。
http://www.ti.com/lit/ug/sniu028a/sniu028a.pdf
谢谢