Other Parts Discussed in Thread: LM3478, TPS61040
使用LM3478制作开关电源。15V升75V 但是输出电流不能满足额定输出电流。不能达到20mA。电路图如下:
请问。负载电流除了和电感的值有关系,和RCOMP&Ccomp以及开关频率以及R12 RISEN都有什么关系呢?为什么输出20mA都不能达成呢?PCB如下:
电感使用的是5mm功率电感,额定电流800mV。 二极管额定电流1A.反向电压200V.MOS Vgd=250V,电容使用的是1812的陶瓷电容。负载2.5K功率电阻时,电路会出现吱吱的叫声。电感发出来的。